BasePlateStyleSetting Class¶
-
class
NXOpen.CAE.Xyplot.
BasePlateStyleSetting
¶ Bases:
NXOpen.CAE.Xyplot.BaseSymbolStyleSetting
Represents the base plate display style.
Call
CAE.Xyplot.IDisplayStyle.CommitChange()
to apply style changes to corresponding plot after it’s modified.Not support KF.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FillingColor | Returns or sets the filling color |
OutlineColor | Returns or sets the outline color |
Owner | Returns the owner style |
PointMarker | Returns or sets the point marker |
ShowOutline | Returns or sets a value indicating whether to display the outline |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Property Detail¶
FillingColor¶
-
BasePlateStyleSetting.
FillingColor
¶ Returns or sets the filling color
-------------------------------------
Getter Method
Signature
FillingColor()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillingColor(fillingColor)
Parameters: fillingColor (Id) – New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
OutlineColor¶
-
BasePlateStyleSetting.
OutlineColor
¶ Returns or sets the outline color
-------------------------------------
Getter Method
Signature
OutlineColor()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutlineColor(outlineColor)
Parameters: outlineColor (Id) – New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Owner¶
-
BasePlateStyleSetting.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner()
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
ShowOutline¶
-
BasePlateStyleSetting.
ShowOutline
¶ Returns or sets a value indicating whether to display the outline
-------------------------------------
Getter Method
Signature
ShowOutline()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowOutline(showOutline)
Parameters: showOutline (bool) – New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)