BarColorOption Enumeration

class NXOpen.CAE.Xyplot.BarColorOption

Bases: object

Represents the bar filling color option Enum Members

Enum Member Enum Member Description
Fill
Fill color or contour color with no shading
Hidden
Background color as fill
Shaded
Fill Color or contour color with shading
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.