AxisDBScale Enumeration

class NXOpen.CAE.Xyplot.AxisDBScale

Bases: object

Represents the DB scale for plot Enum Members

Enum Member Enum Member Description
Ten
Db 10
Twenty
Db 20
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.