VelocityImpactDirection Class

class NXOpen.CAE.ResponseSimulation.VelocityImpactDirection

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.CAE.ResponseSimulation.VelocityImpactDirection

New in version NX6.0.0.

Properties

Property Description
DirectionOption Returns or sets the direction option
NodalComponent Returns or sets the selected nodal component
ReverseDirection Returns or sets the option to reverse direction of nodal component or not.
Tag Returns the Tag for this object.
UserDefinedDirection Returns or sets the user-defined direction

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

VelocityImpactDirectionDirectionType Enumeration the direction options for impact
VelocityImpactDirectionNodalComponentType Enumeration the types of nodal component

Property Detail

DirectionOption

VelocityImpactDirection.DirectionOption

Returns or sets the direction option

-------------------------------------

Getter Method

Signature DirectionOption()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DirectionOption(mDirectionOption)

Parameters:mDirectionOption (NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

NodalComponent

VelocityImpactDirection.NodalComponent

Returns or sets the selected nodal component

-------------------------------------

Getter Method

Signature NodalComponent()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NodalComponent(nodalComponent)

Parameters:nodalComponent (NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ReverseDirection

VelocityImpactDirection.ReverseDirection

Returns or sets the option to reverse direction of nodal component or not.

Only valid when direction option is NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType.NodalComponent

-------------------------------------

Getter Method

Signature ReverseDirection()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReverseDirection(reverseDirection)

Parameters:reverseDirection (bool) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

UserDefinedDirection

VelocityImpactDirection.UserDefinedDirection

Returns or sets the user-defined direction

-------------------------------------

Getter Method

Signature UserDefinedDirection()

Returns:
Return type:NXOpen.Direction

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UserDefinedDirection(userDefinedDirection)

Parameters:userDefinedDirection (NXOpen.Direction) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

Validate

VelocityImpactDirection.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.