TranslationalNodalFunctionExcitationBuilderRotationAxisType Enumeration

NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitationBuilder.RotationAxisType is an alias for NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitationBuilderRotationAxisType

class NXOpen.CAE.ResponseSimulation.TranslationalNodalFunctionExcitationBuilderRotationAxisType

Bases: object

Represents the rotation axis type.

Enum Members

Enum Member Enum Member Description
X  
Y  
Z  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.