StrainGageType Enumeration

class NXOpen.CAE.ResponseSimulation.StrainGageType

Bases: object

Specifies the type of Strain Gage Enum Members

Enum Member Enum Member Description
UniAxial
BiAxial
Rosette45DegreeIncrement
Rosette 0-45-90
Rosette60DegreeIncrement
Rosette 0-60-120
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.