RSEventType Enumeration

NXOpen.CAE.ResponseSimulation.RSEvent.Type is an alias for NXOpen.CAE.ResponseSimulation.RSEventType

class NXOpen.CAE.ResponseSimulation.RSEventType

Bases: object

the type of reponse analysis event

Enum Members

Enum Member Enum Member Description
Transient  
Frequency  
Random  
ResponseSpectrum  
Ddam  
Static  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.