RSEventSpacingType Enumeration

NXOpen.CAE.ResponseSimulation.RSEvent.SpacingType is an alias for NXOpen.CAE.ResponseSimulation.RSEventSpacingType

class NXOpen.CAE.ResponseSimulation.RSEventSpacingType

Bases: object

the spacing type.

Enum Members

Enum Member Enum Member Description
Even  
Uneven  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.