RSEventOutputSetting Class¶
-
class
NXOpen.CAE.ResponseSimulation.
RSEventOutputSetting
¶ Bases:
NXOpen.TaggedObject
Reprensents the output setting for an event
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FemGeometrySaveOption | Returns or sets the option to save FEM information with evaluation results. |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
FemGeometrySaveOption¶
-
RSEventOutputSetting.
FemGeometrySaveOption
¶ Returns or sets the option to save FEM information with evaluation results.
The option could not be changed after the event is created.
-------------------------------------
Getter Method
Signature
FemGeometrySaveOption()
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
FemGeometrySaveOption(saveFemGeometry)
Parameters: saveFemGeometry (bool) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)