RSEventCollection Class

class NXOpen.CAE.ResponseSimulation.RSEventCollection

Bases: object

Represents a collection of response analysis event

To obtain an instance of this class, refer to NXOpen.CAE.ResponseSimulation.Manager

New in version NX5.0.0.

Methods

Method Description
CreateEventBuilder Creates a event buider @return
DeleteEvent Deletes an event
FindObject Finds an event with specified event name @return

Method Detail

CreateEventBuilder

RSEventCollection.CreateEventBuilder

Creates a event buider

Signature CreateEventBuilder(raEvent)

Parameters:raEvent (NXOpen.CAE.ResponseSimulation.RSEvent) –
Returns:
Return type:NXOpen.CAE.ResponseSimulation.RSEventBuilder

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

DeleteEvent

RSEventCollection.DeleteEvent

Deletes an event

Signature DeleteEvent(raEvent)

Parameters:raEvent (NXOpen.CAE.ResponseSimulation.RSEvent) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

FindObject

RSEventCollection.FindObject

Finds an event with specified event name

Signature FindObject(name)

Parameters:name (str) –
Returns:
Return type:NXOpen.CAE.ResponseSimulation.RSEvent

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)