NodalFunctionEvalBeamLocation Enumeration

class NXOpen.CAE.ResponseSimulation.NodalFunctionEvalBeamLocation

Bases: object

Specifies beam element evaluation locations for nodal function evaluation Enum Members

Enum Member Enum Member Description
C
Stress Recovery point C on a beam cross section
D
Stress Recovery point D on a beam cross section
E
Stress Recovery point E on a beam cross section
F
Stress Recovery point F on a beam cross section
All
All four Stress Recovery points on a beam cross section
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.