InterpolationMethod Enumeration

class NXOpen.CAE.ResponseSimulation.InterpolationMethod

Bases: object

This enum defines interpolation method Enum Members

Enum Member Enum Member Description
LogLog  
LinearLinear  
LinearLog  
LogLinear  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.