InitialConditionsType Enumeration

NXOpen.CAE.ResponseSimulation.InitialConditions.Type is an alias for NXOpen.CAE.ResponseSimulation.InitialConditionsType

class NXOpen.CAE.ResponseSimulation.InitialConditionsType

Bases: object

Specifies the method to define initial condition

Enum Members

Enum Member Enum Member Description
QuasiStatic  
Zero  
UserDefined  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.