EvaluationParameters Class

class NXOpen.CAE.ResponseSimulation.EvaluationParameters

Bases: NXOpen.TaggedObject

Represents the evaluation parameters for a response simulation meta solution

Not support KF.

New in version NX6.0.0.

Properties

Property Description
HypermatrixBufferSize Returns or sets the buffer allocated for Hypermatrix files
IntegrationMethod Returns or sets the integration method used for transient analysis
MaxArraySize Returns or sets the dynamic storage array size allocated for RS evaluations
MinDampingStatus Returns or sets the minimum damping ratio status
Tag Returns the Tag for this object.
ZeroMeanCorrection Returns or sets the time-domain integration of acceleration excitations, used in evaluating time responses to acceleration loads.

Methods

Enumerations

EvaluationParametersAnalysisIntegrationMethod Enumeration the integration method used for transient analysis

Property Detail

HypermatrixBufferSize

EvaluationParameters.HypermatrixBufferSize

Returns or sets the buffer allocated for Hypermatrix files

-------------------------------------

Getter Method

Signature HypermatrixBufferSize()

Returns:
Return type:int

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature HypermatrixBufferSize(bufferSize)

Parameters:bufferSize (int) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

IntegrationMethod

EvaluationParameters.IntegrationMethod

Returns or sets the integration method used for transient analysis

-------------------------------------

Getter Method

Signature IntegrationMethod()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature IntegrationMethod(method)

Parameters:method (NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

MaxArraySize

EvaluationParameters.MaxArraySize

Returns or sets the dynamic storage array size allocated for RS evaluations

-------------------------------------

Getter Method

Signature MaxArraySize()

Returns:
Return type:int

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature MaxArraySize(maxArraySize)

Parameters:maxArraySize (int) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

MinDampingStatus

EvaluationParameters.MinDampingStatus

Returns or sets the minimum damping ratio status

-------------------------------------

Getter Method

Signature MinDampingStatus()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature MinDampingStatus(dampingStatus)

Parameters:dampingStatus (bool) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ZeroMeanCorrection

EvaluationParameters.ZeroMeanCorrection

Returns or sets the time-domain integration of acceleration excitations, used in evaluating time responses to acceleration loads.

false: no correction, meaning that “rigid drifting” shows in the displacement response when an acceleration excitation is applied; true: the software corrects for drifting by assuming a zero mean. Rigid drifting is filtered out based on a numerical integration that does not assume an initial condition.

-------------------------------------

Getter Method

Signature ZeroMeanCorrection()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ZeroMeanCorrection(correctionValue)

Parameters:correctionValue (bool) –

New in version NX6.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)