DDAMExcitationShipType Enumeration

NXOpen.CAE.ResponseSimulation.DDAMExcitation.ShipType is an alias for NXOpen.CAE.ResponseSimulation.DDAMExcitationShipType

class NXOpen.CAE.ResponseSimulation.DDAMExcitationShipType

Bases: object

Specifies the ship type

Enum Members

Enum Member Enum Member Description
Surface  
Submarine  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.