DDAMExcitationResponseType Enumeration

NXOpen.CAE.ResponseSimulation.DDAMExcitation.ResponseType is an alias for NXOpen.CAE.ResponseSimulation.DDAMExcitationResponseType

class NXOpen.CAE.ResponseSimulation.DDAMExcitationResponseType

Bases: object

Specifies the response type

Enum Members

Enum Member Enum Member Description
Elastic  
ElasticPlastic  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.