DDAMExcitationCoefficientDefinitionType Enumeration¶
NXOpen.CAE.ResponseSimulation.DDAMExcitation.CoefficientDefinitionType is an alias for NXOpen.CAE.ResponseSimulation.DDAMExcitationCoefficientDefinitionType
-
class
NXOpen.CAE.ResponseSimulation.
DDAMExcitationCoefficientDefinitionType
¶ Bases:
object
the choices of define DDAM coefficients.
Enum Members
Enum Member Enum Member Description ByFile Get the DDAM coefficients from a DDAM coefficient fileInputManually Input the DDAM coefficient manually-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-