TBSTopologyLinkConditionSymmetryOption Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyLinkCondition.SymmetryOption is an alias for NXOpen.CAE.Optimization.TBSTopologyLinkConditionSymmetryOption
-
class
NXOpen.CAE.Optimization.
TBSTopologyLinkConditionSymmetryOption
¶ Bases:
object
Defines the type of link condition
Enum Members
- perpendicular to the given axis of the coordinate system”
- “CyclicSymmetry”, ” Cyclic symmetry definition “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.