TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParameters.VolumeDefinitionMethod is an alias for NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod
-
class
NXOpen.CAE.Optimization.
TBSTopologyControllerOptimizationParametersVolumeDefinitionMethod
¶ Bases:
object
Represents the definition of volume that can be removed immediatedly in the first design cycle
Enum Members
Enum Member Enum Member Description Percent Specifying the volume in percentageAbsolute Specifying the absolute volume-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-