TBSTopologyControllerOptimizationParametersAutoFrozen Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParameters.AutoFrozen is an alias for NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersAutoFrozen
-
class
NXOpen.CAE.Optimization.
TBSTopologyControllerOptimizationParametersAutoFrozen
¶ Bases:
object
Defines the automatic fromzen strategy
Enum Members
Enum Member Enum Member Description Load All loaded elements and nodes are excluded from the optimizationOff Loaded elements are optimizableSpc Elements with boundary conditions are excluded from the optimizationBoth All loaded elements, elements with load nodes with boundary conditions are excluded from the optimization-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-