TBSStopCondition Class¶
-
class
NXOpen.CAE.Optimization.
TBSStopCondition
¶ Bases:
NXOpen.TaggedObject
Represents the condtion to end an optimization
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
MaximumIterationNumber | Returns or sets the maximum number of iteration during the optimization |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
MaximumIterationNumber¶
-
TBSStopCondition.
MaximumIterationNumber
¶ Returns or sets the maximum number of iteration during the optimization
-------------------------------------
Getter Method
Signature
MaximumIterationNumber()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumIterationNumber(iterationNumber)
Parameters: iterationNumber (int) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)