TBSSmoothBuilderSelfIntersectionCheckingOption Enumeration¶
NXOpen.CAE.Optimization.TBSSmoothBuilder.SelfIntersectionCheckingOption is an alias for NXOpen.CAE.Optimization.TBSSmoothBuilderSelfIntersectionCheckingOption
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilderSelfIntersectionCheckingOption
¶ Bases:
object
Defines if the self-itersection checks are to be performed during the isocut, smoothing and data reduction
Enum Members
Enum Member Enum Member Description Off No checksCheck Check onceRuntime Check alwaysIterative First run without check, then rerun if self-intersections are found-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-