TBSSmoothBuilderResultFiltering Enumeration¶
NXOpen.CAE.Optimization.TBSSmoothBuilder.ResultFiltering is an alias for NXOpen.CAE.Optimization.TBSSmoothBuilderResultFiltering
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilderResultFiltering
¶ Bases:
object
Defines if the element material values are to be filtered before the isocut
Enum Members
Enum Member Enum Member Description Off Don’t filter the element material valuesModerate Filters the element material values partiallyFull Filters the element material values fully-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-