TBSSmoothBuilderOriginalSurfaceSmoothingOption Enumeration¶
NXOpen.CAE.Optimization.TBSSmoothBuilder.OriginalSurfaceSmoothingOption is an alias for NXOpen.CAE.Optimization.TBSSmoothBuilderOriginalSurfaceSmoothingOption
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilderOriginalSurfaceSmoothingOption
¶ Bases:
object
Defines if the original surface is to be smoothed or remain unchanged
Enum Members
Enum Member Enum Member Description Off No changes to the original surfaceShrink Allows the nodes on original surface to be moved towards the inside onlyFull Allows any modifications to the original surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-