TBSSmoothBuilderIsoType Enumeration¶
NXOpen.CAE.Optimization.TBSSmoothBuilder.IsoType is an alias for NXOpen.CAE.Optimization.TBSSmoothBuilderIsoType
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilderIsoType
¶ Bases:
object
Specifies the content saved to the output files
Enum Members
Enum Member Enum Member Description Original Saves the original surfaceNew Saves the surface gererated by IsocutBoth Saves the complete surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-