TBSSmoothBuilderFormat Enumeration¶
NXOpen.CAE.Optimization.TBSSmoothBuilder.Format is an alias for NXOpen.CAE.Optimization.TBSSmoothBuilderFormat
-
class
NXOpen.CAE.Optimization.
TBSSmoothBuilderFormat
¶ Bases:
object
Defines the output file format of surface representation
Enum Members
Enum Member Enum Member Description Bdf Represents surfaces in .bdf fileStl Represents surfaces in .stl fileIges Represents surfaces in .igs file-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-