TBSOutputControlOptions Class¶
-
class
NXOpen.CAE.Optimization.
TBSOutputControlOptions
¶ Bases:
NXOpen.TaggedObject
Represents the output result control options of the optimization
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CustomScratchDirectory | Returns or sets the custom cratch directory for solving |
HasCustomScratchDirectory | Returns or sets whether to use a custom cratch directory or not when solving |
IsJobRunInForeground | Returns or sets whether to run optimization job in foreground or not when solving |
Op2OutputOption | Returns or sets the op2 output control option |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TBSOutputControlOptionsOp2Option Enumeration | Defines the op2 output option |
Property Detail¶
CustomScratchDirectory¶
-
TBSOutputControlOptions.
CustomScratchDirectory
¶ Returns or sets the custom cratch directory for solving
-------------------------------------
Getter Method
Signature
CustomScratchDirectory()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomScratchDirectory(customScrathDir)
Parameters: customScrathDir (str) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
HasCustomScratchDirectory¶
-
TBSOutputControlOptions.
HasCustomScratchDirectory
¶ Returns or sets whether to use a custom cratch directory or not when solving
-------------------------------------
Getter Method
Signature
HasCustomScratchDirectory()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HasCustomScratchDirectory(hasCustomScrathDir)
Parameters: hasCustomScrathDir (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
IsJobRunInForeground¶
-
TBSOutputControlOptions.
IsJobRunInForeground
¶ Returns or sets whether to run optimization job in foreground or not when solving
-------------------------------------
Getter Method
Signature
IsJobRunInForeground()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsJobRunInForeground(isJobRunInForeground)
Parameters: isJobRunInForeground (bool) – New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Op2OutputOption¶
-
TBSOutputControlOptions.
Op2OutputOption
¶ Returns or sets the op2 output control option
-------------------------------------
Getter Method
Signature
Op2OutputOption()
Returns: Return type: NXOpen.CAE.Optimization.TBSOutputControlOptionsOp2Option
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Op2OutputOption(op2Option)
Parameters: op2Option ( NXOpen.CAE.Optimization.TBSOutputControlOptionsOp2Option
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)