TBSObjectivesObjectiveType Enumeration¶
NXOpen.CAE.Optimization.TBSObjectives.ObjectiveType is an alias for NXOpen.CAE.Optimization.TBSObjectivesObjectiveType
-
class
NXOpen.CAE.Optimization.
TBSObjectivesObjectiveType
¶ Bases:
object
Defines the target type of the design objective
Enum Members
Enum Member Enum Member Description Minimum Target is to minimize the list of design responseMaximum Target is to maximize the list of design responseMaxMin Target is the MINMAX formulation of the list of design responses-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-