TBSMeshSmoothStrategy Enumeration¶
NXOpen.CAE.Optimization.TBSMeshSmooth.Strategy is an alias for NXOpen.CAE.Optimization.TBSMeshSmoothStrategy
-
class
NXOpen.CAE.Optimization.
TBSMeshSmoothStrategy
¶ Bases:
object
Specify the strategy of mesh smooth
Enum Members
Enum Member Enum Member Description ConstrainedLaplacian Constrained Laplacian StrategyLocalGradient Local Gradient Strategy-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-