TBSLoadCaseLayerOption Enumeration¶
NXOpen.CAE.Optimization.TBSLoadCase.LayerOption is an alias for NXOpen.CAE.Optimization.TBSLoadCaseLayerOption
-
class
NXOpen.CAE.Optimization.
TBSLoadCaseLayerOption
¶ Bases:
object
Defines the location for calcuating shell stresses
Enum Members
Enum Member Enum Member Description NotSet No calculationMaximum the maximum value among Top, Middle and BottomMinimum the minimum value among Top, Middle and BottomTop Top-layer of shellMiddle Mid-layer of shellBottom Bottom layer of shell-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-