TBSDesignResponseBuilderResponse Enumeration¶
NXOpen.CAE.Optimization.TBSDesignResponseBuilder.Response is an alias for NXOpen.CAE.Optimization.TBSDesignResponseBuilderResponse
-
class
NXOpen.CAE.Optimization.
TBSDesignResponseBuilderResponse
¶ Bases:
object
Defines the design response type
Enum Members
Enum Member Enum Member Description DynamicFrequency Eigenfrequency from modal analysisDynamicFrequencyKressissel Eigenfrequency calculated with Kreisselmaier-Steinhauser formulaVolume Volume of elementVolumeFill Volume of elementWeight Weight of elementDisplacementAbsolute Absolute nodal displacementDisplacementX Nodal displacement in X-directionDisplacementY Nodal displacement in Y-directionDisplacementZ Nodal displacement in Z-directionDisplacementXAbsolute Absolute nodal displacement in X-directionDisplacementYAbsolute Absolute nodal displacement in Y-directionDisplacementZAbsolute Absolute nodal displacement in Z-directionmRotationAbsolute Absolute rotationRotationX Nodal rotation around X-axisRotationY Nodal rotation around Y-axisRotationZ Nodal rotation around Z-axisRotationXAbsolute Absolute nodal rotation around X-axisRotationYAbsolute Absolute nodal rotation around Y-axisRotationZAbsolute Absolute nodal rotation around Z-axisStrainEnergy Strain energyCenterGravityX Center of gravity for the X-directionCenterGravityY Center of gravity for the Y-directionCenterGravityZ Center of gravity for the Z-directionInertiaXx Moment of inertia around X-X-directionInertiaXy Moment of inertia around X-Y-directionInertiaXz Moment of inertia around X-Z-directionInertiaYy Moment of inertia around Y-Y-directionInertiaYz Moment of inertia around Y-Z-directionInertiaZz Moment of inertia around Z-Z-directionReactionForceAbsolute Absolute nodal reaction forceReactionForceX Nodal reaction force in X-directionReactionForceY Nodal reaction force in Y-directionReactionForceZ Nodal reaction force in Z-directionReactionForceXAbsolute Absolute nodal reaction force in X-directionReactionForceYAbsolute Absolute nodal reaction force in Y-directionReactionForceZAbsolute Absolute nodal reaction force in Z-directionReactionForceRotationAbsolute Absolute nodal reaction momentReactionForceRotationX Nodal reaction moment around X-axisReactionForceRotationY Nodal reaction moment around Y-axisReactionForceRotationZ Nodal reaction moment around Z-axisReactionForceRotationXAbsolute Absolute nodal reaction moment around X-axisReactionForceRotationYAbsolute Absolute nodal reaction moment around Y-axisReactionForceRotationZAbsolute Absolute nodal reaction moment around Z-axisInternalForceAbsolute Absolute nodal internal forceInternalForceX Nodal internal force in X-directionInternalForceY Nodal internal force in Y-directionInternalForceZ Nodal internal force in Z-directionInternalForceXAbsolute Absolute nodal internal force in X-directionInternalForceYAbsolute Absolute nodal internal force in Y-directionInternalForceZAbsolute Absolute nodal internal force in Z-directionInternalForceRotationAbsolute Absolute nodal internal momentInternalForceRotationX Nodal internal moment around X-axisInternalForceRotationY Nodal internal moment around Y-axisInternalForceRotationZ Nodal internal moment around Z-axisInternalForceRotationXAbsolute Absolute nodal internal moment around X-axisInternalForceRotationYAbsolute Absolute nodal internal moment around Y-axisInternalForceRotationZAbsolute Absolute nodal internal moment around Z-axisFrequencyResponseAccelerationX Acceleration in X-direction for frequency responseFrequencyResponseAccelerationY Acceleration in Y-direction for frequency responseFrequencyResponseAccelerationZ Acceleration in Z-direction for frequency responseFrequencyResponseCompliance Dynamic compliance for frequency responseFrequencyResponseDbaPressure Sound pressure level (dBA)FrequencyResponseDbPressure Sound pressure level (dB)FrequencyResponseDisplacementAbsolute Absolute amplitude for frequency responseFrequencyResponseDisplacementXAbsolute Amplitude in X-direction for frequency responseFrequencyResponseDisplacementYAbsolute Amplitude in Y-direction for frequency responsFrequencyResponseDisplacementZAbsolute Amplitude in Z-direction for frequency responsFrequencyResponsePhaseXAbsolute Phase in X-direction for frequency responseFrequencyResponsePhaseYAbsolute Phase in Y-direction for frequency responseFrequencyResponsePhaseZAbsolute Phase in Z-direction for frequency responseFrequencyResponsePressure Instantaneous sound pressureFrequencyResponseRmsPressure Effective sound pressureFrequencyResponseVelocityXAbsolute Velocity in X-direction for frequecy responseFrequencyResponseVelocityYAbsolute Velocity in Y-direction for frequecy responseFrequencyResponseVelocityZAbsolute Velocity in Z-direction for frequecy responseFrequencyResponseNvhSolid Surface normal velocity equivalent. Referenced node group, must be on solid elementsFrequencyResponseNvhShell Surface normal velocity equivalent. Referenced node group, must be on plate or shell elementsMisesStressHypothesis Mises Stress hypothesisMaximumPrincipalStress Maximum principal StressMinimumAbsolutePrincipalStress Absolute value of the minimum principal StressMaximumAbsolutePrincipalStress Maximum of absolute value of the principal stress-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-