TBSBaseDesignVariableBuilderGroupOperator Enumeration¶
NXOpen.CAE.Optimization.TBSBaseDesignVariableBuilder.GroupOperator is an alias for NXOpen.CAE.Optimization.TBSBaseDesignVariableBuilderGroupOperator
-
class
NXOpen.CAE.Optimization.
TBSBaseDesignVariableBuilderGroupOperator
¶ Bases:
object
Defines the operator type to determine the design variable that used within the selection area
Enum Members
Enum Member Enum Member Description Max Maximum value fo the selection areaMin Minimum value of the selection areaSum Sum of all values of the selection areaCount Determines the number of values of the selection areaDeviation Deviation from the maximum value of the reference value-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-