DAOStopCondition Class¶
-
class
NXOpen.CAE.Optimization.
DAOStopCondition
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.CAE.Optimization.DAOStopCondition
.New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AbsoluteConvergence | Returns or sets the absolute convergence |
ConstraintChecking | Returns or sets the constraint checking flag, only effective for global sensitivity optimization type |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaxConstraintViolation | Returns or sets the maximum constraint violation |
MaxIterations | Returns or sets the maximum iteration number |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PerturbationFraction | Returns or sets the perturbation fraction |
Prototype | Returns the prototype of this object if it is an occurrence. |
RelativeConvergence | Returns or sets the relative convergence |
SaveAllIterationResults | Returns or sets the save all interation results flag |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
AbsoluteConvergence¶
-
DAOStopCondition.
AbsoluteConvergence
¶ Returns or sets the absolute convergence
-------------------------------------
Getter Method
Signature
AbsoluteConvergence()
Returns: Absolute convergence Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AbsoluteConvergence(absoluteConvergence)
Parameters: absoluteConvergence (float) – Absolute convergence New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ConstraintChecking¶
-
DAOStopCondition.
ConstraintChecking
¶ Returns or sets the constraint checking flag, only effective for global sensitivity optimization type
-------------------------------------
Getter Method
Signature
ConstraintChecking()
Returns: Constraint checking flag Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstraintChecking(constraintChecking)
Parameters: constraintChecking (bool) – Constraint checking flag New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
DAOStopCondition.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DAOStopCondition.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaxConstraintViolation¶
-
DAOStopCondition.
MaxConstraintViolation
¶ Returns or sets the maximum constraint violation
-------------------------------------
Getter Method
Signature
MaxConstraintViolation()
Returns: Maximum constraint violation Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxConstraintViolation(constraintViolation)
Parameters: constraintViolation (float) – Maximum constraint violation New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
MaxIterations¶
-
DAOStopCondition.
MaxIterations
¶ Returns or sets the maximum iteration number
-------------------------------------
Getter Method
Signature
MaxIterations()
Returns: Step number Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxIterations(stepNumber)
Parameters: stepNumber (int) – Step number New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
DAOStopCondition.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
DAOStopCondition.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DAOStopCondition.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PerturbationFraction¶
-
DAOStopCondition.
PerturbationFraction
¶ Returns or sets the perturbation fraction
-------------------------------------
Getter Method
Signature
PerturbationFraction()
Returns: Perturbation fraction Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PerturbationFraction(perturbationFraction)
Parameters: perturbationFraction (float) – Perturbation fraction New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
DAOStopCondition.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
RelativeConvergence¶
-
DAOStopCondition.
RelativeConvergence
¶ Returns or sets the relative convergence
-------------------------------------
Getter Method
Signature
RelativeConvergence()
Returns: Relative convergence Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelativeConvergence(relativeConvergence)
Parameters: relativeConvergence (float) – Relative convergence New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SaveAllIterationResults¶
-
DAOStopCondition.
SaveAllIterationResults
¶ Returns or sets the save all interation results flag
-------------------------------------
Getter Method
Signature
SaveAllIterationResults()
Returns: Save all iteration results flag Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveAllIterationResults(saveResults)
Parameters: saveResults (bool) – Save all iteration results flag New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
FindObject¶
-
DAOStopCondition.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
DAOStopCondition.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
DAOStopCondition.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.