TestValueTypesValidator Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.Validator is an alias for NXOpen.CAE.ModelCheck.TestValueTypesValidator
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesValidator
¶ Bases:
object
indicates how to compare the check result with the criteria value
Enum Members
Enum Member Enum Member Description NotSet indicates no criteria value defined, not necessary to compare the check result with criteria valueGreatThan the check passes if the check result is great than the criteria valueGreatThanOrEqual the check passes if the check result is equal or great than the criteria valueSmallThan the check passes if the check result is small than the criteria valueSmallThanOrEqual the check passes if the check result is equal or small than the criteria value-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-