DuplicateNodesCheckBuilderMergePreference Enumeration¶
NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.MergePreference is an alias for NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilderMergePreference
-
class
NXOpen.CAE.ModelCheck.
DuplicateNodesCheckBuilderMergePreference
¶ Bases:
object
Represents the duplicate nodes merging preference
Enum Members
NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.SelectPreferenceNodesList()
“- “RemoveSelected”, ” Merge the nodes specified in the node list
NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.SelectPreferenceNodesList()
“-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.