DataManagerAfuRecordZValue Enumeration

NXOpen.CAE.FTK.DataManager.AfuRecordZValue is an alias for NXOpen.CAE.FTK.DataManagerAfuRecordZValue

class NXOpen.CAE.FTK.DataManagerAfuRecordZValue

Bases: object

Represents the method to get Z value for afu record in 3D plot

Enum Members

Enum Member Enum Member Description
SelectionOrder
The Z value is selection order
General
The Z value is attribute of General field in an afu record
Rpm
The z value is attribute of RPM field in an afu record
Time
The z value is attribute of Time field in an afu record
Order
The z value is attribute of Order field in an afu record
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.