FEModelOccurrence Class¶
-
class
NXOpen.CAE.
FEModelOccurrence
¶ Bases:
NXOpen.CAE.IFEModel
,NXOpen.CAE.IHierarchicalFEModel
This class represents a Finite Element Model Occurrence. Only one instance of this class will exist in each sim part file
An instance of this class can not be obtained
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FeelementLabelMap | Returns a CAE.FEElement Label to CAE.FEElement Map for this Interface to the Finite Element Model. |
FenodeLabelMap | Returns a CAE.FENode Label to CAE.FENode Map for this Interface to the Finite Element Model. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MeshManager | Returns the IMeshManager |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Parent | Returns the parent fem of this object, can be None |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Find | Finds the object within the NXOpen.CAE.FEModelOccurrence context, with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetAttributes | Get the femodel occurrence attributes @return |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildren | Returns the child components of this component @return |
GetComponent | Gets the NXOpen.Assemblies.Component associated with this object @return |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLabelOffsets | Returns node, element, and csys offset of the femodel occurrence |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetLabelOffsets | Sets node, element, and csys offset of the femodel occurrence |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
FEModelOccurrence.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FEModelOccurrence.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FEModelOccurrence.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FEModelOccurrence.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FEModelOccurrence.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Parent¶
-
FEModelOccurrence.
Parent
¶ Returns the parent fem of this object, can be None
-------------------------------------
Getter Method
Signature
Parent()
Returns: The parent Return type: NXOpen.CAE.IFEModel
New in version NX6.0.0.
License requirements: None.
Prototype¶
-
FEModelOccurrence.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Find¶
-
FEModelOccurrence.
Find
¶ Finds the object within the
NXOpen.CAE.FEModelOccurrence
context, with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Object with the journal identifier Return type: NXOpen.TaggedObject
New in version NX3.0.0.
License requirements: None.
FindObject¶
-
FEModelOccurrence.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAttributes¶
-
FEModelOccurrence.
GetAttributes
¶ Get the femodel occurrence attributes
Signature
GetAttributes()
Returns: Return type: NXOpen.CAE.FEModelOccAttribute
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetChildren¶
-
FEModelOccurrence.
GetChildren
¶ Returns the child components of this component
Signature
GetChildren()
Returns: Return type: list of NXOpen.CAE.FEModelOccurrence
New in version NX6.0.0.
License requirements: None.
GetComponent¶
-
FEModelOccurrence.
GetComponent
¶ Gets the
NXOpen.Assemblies.Component
associated with this objectSignature
GetComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX6.0.0.
License requirements: None.
GetLabelOffsets¶
-
FEModelOccurrence.
GetLabelOffsets
¶ Returns node, element, and csys offset of the femodel occurrence
Signature
GetLabelOffsets()
Returns: a tuple Return type: A tuple consisting of (nodeOffset, elemOffset, csysOffset). nodeOffset is a int. node offset elemOffset is a int. element offset csysOffset is a int. csys offset New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Print¶
-
FEModelOccurrence.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetLabelOffsets¶
-
FEModelOccurrence.
SetLabelOffsets
¶ Sets node, element, and csys offset of the femodel occurrence
Signature
SetLabelOffsets(nodeOffset, elemOffset, csysOffset)
Parameters: - nodeOffset (int) – node offset
- elemOffset (int) – element offset
- csysOffset (int) – csys offset
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetName¶
-
FEModelOccurrence.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.