OnestepUnformBuilderUnfoldMode Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.UnfoldMode is an alias for NXOpen.BodyDes.OnestepUnformBuilderUnfoldMode

class NXOpen.BodyDes.OnestepUnformBuilderUnfoldMode

Bases: object

The Onesetp unfold mode of onestep unform.

Enum Members

Enum Member Enum Member Description
Complete
Onestep unfold mode is complete
Intermediate
Onestep unfold mode is intermediate
Unknown
Onestep unfold mode is unknown
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.