OnestepUnformBuilderSurface Enumeration¶
NXOpen.BodyDes.OnestepUnformBuilder.Surface is an alias for NXOpen.BodyDes.OnestepUnformBuilderSurface
-
class
NXOpen.BodyDes.
OnestepUnformBuilderSurface
¶ Bases:
object
The surface types of onestep unform.
Enum Members
Enum Member Enum Member Description Inner Onestep solver will offset inner surface and enlarge it Middle Onestep solver will not offset middle surface Outer Onestep solver will offset outer surface and shrink it -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-