OnestepUnformBuilderProcess Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.Process is an alias for NXOpen.BodyDes.OnestepUnformBuilderProcess

class NXOpen.BodyDes.OnestepUnformBuilderProcess

Bases: object

The process types of onestep unform.

Enum Members

Enum Member Enum Member Description
EntireUnform entire
IntermediateUnform intermediate
AdvancedUnform spring back
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.