OnestepUnformBuilderConstraint Enumeration¶
NXOpen.BodyDes.OnestepUnformBuilder.Constraint is an alias for NXOpen.BodyDes.OnestepUnformBuilderConstraint
-
class
NXOpen.BodyDes.
OnestepUnformBuilderConstraint
¶ Bases:
object
The constraints of onestep unform.
Enum Members
Enum Member Enum Member Description CurveToCurve Curve to Curve Constraint, used for intermediate unform only PointToPoint Point to Point Constraint, used for complete unform only CurveAlongCurve Curve along Curve Constraint, used for complete unform only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-