TreeNodeInsertOption Enumeration¶
NXOpen.BlockStyler.Tree.NodeInsertOption is an alias for NXOpen.BlockStyler.TreeNodeInsertOption
-
class
NXOpen.BlockStyler.
TreeNodeInsertOption
¶ Bases:
object
Represents the node insert option which is used while inserting the node in tree.
Enum Members
BlockStyler.TreeNodeInsertOption.First
, except that it remains first after a column sort. If there is more than one node beneath a single parent with this option then they will be sorted relative to each other. ““AlwaysLast”, “Node is placed last in the hierarchy in which it is inserted. This is same asBlockStyler.TreeNodeInsertOption.Last
, except that it remains last after a column sort. If there is more than one node beneath a single parent with this option then they will be sorted relative to each other. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-