TreeEndLabelEditState Enumeration

NXOpen.BlockStyler.Tree.EndLabelEditState is an alias for NXOpen.BlockStyler.TreeEndLabelEditState

class NXOpen.BlockStyler.TreeEndLabelEditState

Bases: object

Represents the state to accept/reject the edited label of node.

Use these options in callback BlockStyler.Tree.OnEndLabelEditCallback.

Enum Members

Enum Member Enum Member Description
AcceptText Use this option to accept the edited text.
RejectText Use this option to reject the edited text and retain the previous one.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.