TreeEditControlOption Enumeration¶
NXOpen.BlockStyler.Tree.EditControlOption is an alias for NXOpen.BlockStyler.TreeEditControlOption
-
class
NXOpen.BlockStyler.
TreeEditControlOption
¶ Bases:
object
Represents the options to accept or reject the changed value.
Enum Members
Enum Member Enum Member Description Accept Use this option to allow edit. Reject Use this option to disallow edit. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-