TreeBeginLabelEditState Enumeration¶
NXOpen.BlockStyler.Tree.BeginLabelEditState is an alias for NXOpen.BlockStyler.TreeBeginLabelEditState
-
class
NXOpen.BlockStyler.
TreeBeginLabelEditState
¶ Bases:
object
Represents the state to allow/disallow the node label edit.
Use these options in callback BlockStyler.Tree.OnBeginLabelEditCallback.
Enum Members
Enum Member Enum Member Description Allow Use this option to allow label edit. Disallow Use this option to disallow label edit. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-