SetListInsertionLocation Enumeration

NXOpen.BlockStyler.SetList.InsertionLocation is an alias for NXOpen.BlockStyler.SetListInsertionLocation

class NXOpen.BlockStyler.SetListInsertionLocation

Bases: object

During Insert, indicates whether component should be inserted before or after the insertion location

Enum Members

Enum Member Enum Member Description
Before
After
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.