PropertyListPropertyType Enumeration¶
NXOpen.BlockStyler.PropertyList.PropertyType is an alias for NXOpen.BlockStyler.PropertyListPropertyType
-
class
NXOpen.BlockStyler.
PropertyListPropertyType
¶ Bases:
object
Represents the property types.
Enum Members
Enum Member Enum Member Description String String Double Double Logical Logical Integer Integer Enum Enum Strings Strings UIBlock UIBlock Point Point Vector Vector Bits Bits TaggedObject Tagged Object Array Array IntegerMatrix2d Integer 2d-Matrix DoubleMatrix2d Double 2d-Matrix TaggedObjectMatrix2d Tagged Object 2d-Matrix IntegerVector Integer Vector DoubleVector Double Vector TaggedObjectVector Tagged Object Vector File File SelectionFilter Selection Filter Undefined Undefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-