PropertyListListMode Enumeration¶
NXOpen.BlockStyler.PropertyList.ListMode is an alias for NXOpen.BlockStyler.PropertyListListMode
-
class
NXOpen.BlockStyler.
PropertyListListMode
¶ Bases:
object
Indicates whether the properties in the list are named.
Enum Members
- must be indexed through an integer index “
- “Named”, ” The properties are named “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.