ChooseExpression Class¶
-
class
NXOpen.BlockStyler.
ChooseExpression
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents Choose Expression block
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
ExpressionSortTypeAsString | Returns or sets the ExpressionSortType as string |
ExpressionTypeIndexAsString | Returns or sets the ExpressionTypeIndex as string |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
Name | Returns the name of the block or BlockID |
SelectedExpression | Returns or sets the SelectedExpression |
Show | Returns or sets the Visibility of block. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetExpressionSortTypeMembers | Gets the ExpressionSortType members @return |
GetExpressionTypeIndexMembers | Gets the ExpressionTypeIndex members @return |
GetProperties | Returns the properties of the block @return |
Property Detail¶
ExpressionSortTypeAsString¶
-
ChooseExpression.
ExpressionSortTypeAsString
¶ Returns or sets the ExpressionSortType as string
-------------------------------------
Getter Method
Signature
ExpressionSortTypeAsString()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExpressionSortTypeAsString(enumString)
Parameters: enumString (str) – New in version NX8.5.0.
License requirements: None.
ExpressionTypeIndexAsString¶
-
ChooseExpression.
ExpressionTypeIndexAsString
¶ Returns or sets the ExpressionTypeIndex as string
-------------------------------------
Getter Method
Signature
ExpressionTypeIndexAsString()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExpressionTypeIndexAsString(enumString)
Parameters: enumString (str) – New in version NX8.5.0.
License requirements: None.
SelectedExpression¶
-
ChooseExpression.
SelectedExpression
¶ Returns or sets the SelectedExpression
-------------------------------------
Getter Method
Signature
SelectedExpression()
Returns: Return type: NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedExpression(selectedExpression)
Parameters: selectedExpression ( NXOpen.TaggedObject
) –New in version NX8.5.0.
License requirements: None.