ObjectBuilderWave Enumeration

NXOpen.Assemblies.ProductInterface.ObjectBuilder.Wave is an alias for NXOpen.Assemblies.ProductInterface.ObjectBuilderWave

class NXOpen.Assemblies.ProductInterface.ObjectBuilderWave

Bases: object

An enum representing settings available for rule checking during creation of WAVE geomtery and interpart expressions

Enum Members

Enum Member Enum Member Description
NoCheck
no checking for product interface objects
Warn
warn user while using non product interface objects
Prevent
restrict user from using non product interface objects
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.